AD9284
Recommended for New Designs
The AD9284 is a dual 8-bit, monolithic sampling, analog-to-digital converter (ADC) that supports simultaneous operation and is optimized for low cost,...
Datasheet
AD9284 on Analog.com
Hi, I designed 4CH board with AD9284 ADC. Attached below is one channel with ADC driver AD4937 and AD9284 IC, but there are 3 other identical channels also. The problem Im having is output LVDS common mode voltage is low when I probe output data or clock lines on any of the 4 ADC ICs. I verified that the ADC driver is working as expected, there is 250MHz input clock on all 4 ADCs, and OE pin is in logic low state as it should be.
DC level Im measuring on all 36 output LVDS lines is around ~150mV, I need to mention that the FMC card with ADCs is connected to Xilinx AC701 Artix 7 eval board with FPGA unconfigured, all inputs to FPGA are tri-state and unterminated. I dont know if this would affect AD9284 LVDS output common mode voltage because I thought that about 1.2V common mode voltage should be present on all 36 LVDS pairs even if they are not connected to any LVDS receiver.
Can you please tell me if this is normal behavior?
Thanks

Hi amelie,
Thank you for your interest in AD9284.
The typical behavior of the LVDS output would be around 1.15-1.35V for output offset voltage and 290-400mV for differential output voltage. Kindly check if the the pin supplies AVDD and DRVDD are both 1.8V and the supply current IDRVDD is around 51mA. Also, can I ask what are the peak-to-peak values of the input signal and the differential signal after the ADC driver?
It seems that there is a mismatch in the input span of the ADC which is 1.2Vpp and the output span of your ADC driver is 2Vpp.

I recommend the following solutions:



Best regards,
Xavier
I checked all power supplies, everything is nominal as it should be. I know it seems there is a mismatch but ADC driver is designed around 50ohm input impedance, so the gain must be set to 2. Input signal gets divided on the input so 1Vpp input is 500mVpp on the input of the ADC driver. As you can see from the picture below purple trace shows differential signal on the input of AD9284, it is 1Vpp.
On all 4 AD9284 ICs analog common mode voltage VCM is 1.68V and not around 1.4V as specified in datasheet, although there isnt any specification of VCM tolerance and drift in the datasheet.
I dont know why there wouldnt be any common mode voltage on all 36 LVDS pairs, because analog system for driving the analog inputs is working as I designed it to be honest, and all power supllies are nominal. There isnt much else on the board except 250MHz clocking subsystem, which also provides correct clock to AD9284s. I can only assume that AD9284 detects there isnt any receiver or termination connected so it tri-states or pulls to ground al LVDS pins. I didnt create FPGA design to verify this yet so Im asking here if that is maybe the problem.
Thanks
Hi amelie,
Thanks for your response. With regards to FPGA, it will constitute as a problem to the LVDS output if it is not configured properly.
I suggest the following recommendations:
![]()
I also included the user guide of the AD9284 evaluation board for your schematic reference. AD9284-250EBZ_UG-178 (Rev. A) (analog.com) Moreover, if you have other prototype boards, please check if it encounter the same problem. Sharing with you below are snippets from our evaluation board. Hope this will help.


Regards,
Xavier
Hi, my schematic agrees with eval schematic so that is ok, bare AD9284 without any fpga connected shows voltage of 300mV DC at all LVDS outputs.
But maybe you have found a solution, register 0x14 seems to initialize to 0x00 at reset, and that means that outputs are disabled because enable need to be at 1, is that correct? I thought that default reset configuration is ok for my use case, but it seems that I missed bit4 in 0x14 register, if bit4 needs to be 1, that is most certainly the problem. I need just to verify this.
Thanks