Post Go back to editing

AD9201 maximum input voltage on the Analog Input pins

I am working through a design where that output of a RF detector circuit with a differential output is to be sampled by the AD9201. It is not my design, but I am responsible for figuring out what is not working correctly.

The output of the detector is converted to differential using a couple of operational amplifiers. On the output of each amplifier is a series 150 ohm resistor at about 6.33mA resulting in each output going from 0 to 1V and 0 to -1V.

Differential Output

The differential signals are filtered (6 MHz LPF) and then scaled by an AD8137. The output of the op amp ranges from 1.5V to 2.5V (1V differential).

The next step is using the AD9201 to sample the differential signal.

Here is where I think I am having issues.The designer is using two external resistors to set the Vref voltage to 2.43V with a span of 2.43V.

What I need validation on is the datasheet specifies the ANALOG INPUT voltage range to be from -0.5 to AVDD/2 (5V/2 = 2.5V). The FPGA designer says that he is only seeing 4 or 5 bits ever toggle. So, is this the source of the error. (Our Systems guy has no hardware for me to test my theory but we are going through a board respin and have the chance to fix and verify on the next prototypes.)

Thanks in advance!

  • Whoops. I need to clarify that if the maximum 10-bit full scale is designed for 3.6V, but the ANALOG maximum input is 2.5V, are we stressing the part and is it the result of not getting 10-bits of information?

  • Hi ajelmer,

    Thank you for your interest in AD9201.

    Based on the absolute maximum rating of the analog input pins, the device is not stressed in the configuration. Though, we would like to correct that the Vspan is equal to Vref for programmable reference configuration which is equal to 1+R2/R1 and not 1+R1/R2.

    However, for the toggling concern, the maximum input voltage swing of 2.43V is not fully utilized if the analog input is only 1Vpp.

    To fully utilize the resolution of the ADC, please try any of the following options:

    • Increase the input swing to fully utilize the span, or
    • Change the reference mode to 1V to cater the input swing.

    Regards,

    Xavier 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.