Hi,
I am using my own FPGA board and AD9656 PCB to verify the JESD204B protocol. But I can't get any data with my current configuration. So I have some questions about this AD9656 DATA output config.
(1) By default, the AD9656 would output data without any configuration, is that right?
(2)The default configuration is: M=4, Lane=1, if ADC clk = 100MHz, then, data output rate is 4Gbps, is that right?
(3)The default configuration timing is like below, I want to know where is location of the LSB part, are they following at next clk cycle by the same pattern?
(4)If I use quick config, Setting 0x5E with value 0x44, which mean M=4, Lane=4, clk=100MHz, then what is the data output rate? Is it still 4Gbps?
(5) With qucik config M=4, Lane=4, How does the ADC data map to the JESD204B Lane? Is the picture mapping below correct?