Post Go back to editing

ad9460 impedence question.

this is AD9460 input circuit. this circuit used ADT1-1WT  and 75 ohm, but our circuit use 50 ohm input signal impedance.

In the evaluation board, ETC1-1-13 with 50 ohm impedance was used, but since we use 50 ohm, 1Mhz input signal, ETC1-1-13 using 4.5 ~ 3000Mhz cannot be used.

Can the ADT1-1WT be used in a 50ohm impedance circuit as written on the evaluation board DataSheet?

Also we need a splitter that inverts the signal by 0 and 180 degrees before input to the ad9460. Are there any ICs that AnalogDevice recommends?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.