I am using AD977A/AD976A on my PCB, how much voltage it can sense at the input terminal? As it is coming with an internal reference voltage of 2.5V, can we collect the analogue voltage signal at the input of amplitude 2.5 V - 5V?
AD977A
Not Recommended for New Designs
The AD977 / AD977A is a high speed, low power 16-bit A/D converter that operates from a single 5 V supply. The AD977A has a throughput rate of 200 kSPS...
Datasheet
AD977A on Analog.com
AD976A
Not Recommended for New Designs
The AD976 and AD976A are high-speed, low-power 16-bit A/D converters with each operating from a single 5 V supply. The AD976A has a throughput rate of...
Datasheet
AD976A on Analog.com
I am using AD977A/AD976A on my PCB, how much voltage it can sense at the input terminal? As it is coming with an internal reference voltage of 2.5V, can we collect the analogue voltage signal at the input of amplitude 2.5 V - 5V?
Hi,
As per datasheet. The AD977/AD977A is specified to operate with six full-scale analog input ranges. Connections required for each of the three analog inputs, R1IN, R2IN and R3IN, and the resulting full-scale ranges, are shown in Table I and Table II.

Thanks,
Jellenie
Hi,
Thanks.
I could not find these Table-1, Table-2 in AD976A datasheet. Could you help with that too?
Hi,
Thanks.
I could not find these Table-1, Table-2 in AD976A datasheet. Could you help with that too?
Hi,
You can’t find it as the AD976A is not as flexible as AD977A. For the AD976 the analog input range is
nominally a bipolar –10 V to +10 V. or the full-scale analog input range can be best represented as ± 4 VREF.
Thanks,
Jellenie