Dear Team,
The AD9213 is a Complex ADC or Real ADC. Since by default it uses single converter (M = 1) and 16 lanes.
Thanks in Advance
Goli Ganesh
Dear Team,
The AD9213 is a Complex ADC or Real ADC. Since by default it uses single converter (M = 1) and 16 lanes.
Thanks in Advance
Goli Ganesh
Hi Ganesh_Goli,
Thank you for your interest in AD9213. In default mode (full bandwidth, M = 1), the AD9213 outputs are real.
The AD9213 has a DDC which can output complex values. When using the DDC in complex mode the outputs are complex. M = 2 (virtual converters).
Thank you.
Doug
Hi DougI ,
In AD9213 ADC, what is the purpose of TRIG_x pin. If we want to AD9213 at 10GSps sampling rate is it necessary to use Averaged SYSREF Mode or it is only used for Multi Chip Synchronization purpose only.
Thanks in Advance
Goli Ganesh
Hi,
The TRIG_x pin is used for hopping to/from different frequency profiles.
If you do not need to synchronize multiple AD9213s, you do not need to use Averaged SYSREF mode. Averaged SYSREF mode is for Multi-Chip Synchronization.
Thank you.
Doug
Hi,
The TRIG_x pin is used for hopping to/from different frequency profiles.
If you do not need to synchronize multiple AD9213s, you do not need to use Averaged SYSREF mode. Averaged SYSREF mode is for Multi-Chip Synchronization.
Thank you.
Doug