Hi All,
I'm SK Lee. (in charge of DFAE)
One of my customer is using LTC1605-1CG#TRPBF.
Question) Why 0.8V is probed on Vin (Pin 1) without input signal ?
Background) Customer checked Vin(Pin 1) with a probe while no external signal is applied to Vin(Pin 1), then 0.8V is basically detected. Also, 0.8V is read in the same way even if the register is read using MCU. Customers have to apply a signal from 0.1V to 4V. The problem is that basically 0.8V is detected on Vin (Pin 1). How can we solve this issue ?