Post Go back to editing

ADC Time conversion speed problem

Hi,
I want to read ADC at high speed (Conversion Time=1.1ms) using DC742B Board and Linduino One Board. I connected the DC742B Board and the Linduino One Board with a ribbon cable. I uploaded the DC590B code on github into Linduino One Board. I applied it from the CH1 input of the DC742B Board by making a voltage divider (about 1Volt) with an 18K resistor and a 5K resistor. Then I was able to read this voltage with the QuikEval K114 interface. I read the SPI line of the LTC742B Board with the help of Logic Analyzer. When I selected the Conversion Time option on the QuikEval K114 interface as 36ms, 72ms and 145ms and read the SPI with the logic analyzer, I actually saw that the data was updated at these intervals. However, when I set the Conversion Time option down to less than 36ms (1.1ms, 2.3ms, 4.5ms, 9ms, 18ms), I saw that the data could not be updated at the selected intervals and the data was updated at variable intervals between 21ms-28ms, no matter which of these options is selected. What could be the cause of this problem? 

The above figure shows the Logic Analyzer interface. Here Conversion Time=1.1ms. However, it is seen that the data intervals are around 23ms.

The figure above shows the QuikEval K114 interface.

Thank you.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.