AD9683 dev board FMC pinout

Hello Everybody, 

Looking into the Schematic of AD9683 development board ad9683_final_schematic_02_040310c.pdf I see this:

And looking into the schematic of the recommended host FPGA board HSC-ADC-EVALEZ schematic file, sch_hadv6fmc01d.pdf I see the following:

    

So it seems there is something wrong in one side, that A-K letters are wrong placed. 

I would appreciate if anyone could put a light on this and verify if those two boards are working together.

Or is the AD9683 Board connections REALLY flipped?

Best Regards,

Parents Reply Children
No Data