Post Go back to editing

AD9652 - VREF

Hi,

I want to adjust the voltage of VREF using an external reference.

I couldn't find the specification for VREF in the datasheet.

What is the minimum voltage that can be applied to that external reference (VREF pin) ?

Thanks.

Hello,

The description of the Internal reference suggests that the VREF pin voltage can be varied between 1.0 and 1.25 V via SPI. 
This range should also apply when the internal voltage is disabled and replaced with an external voltage.  So using an external voltage reference of 1.0 V should result in 2.0 V pp which is the lowest full-scale supported.