I want to capture data using the AD9208-3000EBZ with ADS7-V2 with the following setup seen in the screenshot
The issue I am having is that when I try to run the data capture I get an error message stating invalid JESD204B parameter combination. I also am getting JESD link status showing ILAS and CGS errors, and all DS(1-6) lights are on except for DS5
Is this not a valid combination of parameters supported by the AD9208?
On the AD9208-3000EBZ, I have a 2.4 GHz, 10dBm signal going into J201 (sample clock),
and 597.4MHz going into J101 at 0 dBm
On the ADS7-V2 I have a 100 MHz signal going in at 10 dBm (reference clock).
I have the following configuration in the ACE software:
Clock Input: 2.4 GHz, DDC0 on, decimation by 48, real input from channel A, complex output (2 virtual converters)
L = 1, M = 2, F = 1, N' = 16.
Lane line rate = 2Gbps,
Any help is greatly appreciated.