Post Go back to editing

LTC2298-14 ADC and DC890B evaluation board: Store more than 64k sample data

Hello!

        I am sorry to disturb you. I am using the Pscope software LTC2298-14 ADC with DC890B evaluation board. I think the maximum storage data size that can be selected is 65536. I want to use a 10M clock signal to collect 10M+1Hz signals , I need to store more data if I want to see the changes in the collected information. Is there any way to store more than 64K of sample data? The following is the picture collected by my experiment, the first picture is 9M clock samples 10M signal under test; the second figure is 9.999M clock samples 10M signal under test.

Thank you very much!

 

Parents Reply Children
No Data