Post Go back to editing

AD9864 White Noise and Sampling Rate Questions

Hello

I have two questions regarding the AD9864.

question 1
Is there any white noise characteristic data for the AD9864?

Question 2
Please tell me the sampling rate when communicating AD9864 with SSI.

We would appreciate it if you could reply.

Best regards,

Knj

Parents
  • Hello,

    Answers to your questions are as follows:

    1)The white noise contribution is from the LNA/VGA/Mixer while the colored noise contribution is from the sigma delta ADC.  Operating with 24-bit  IQ data can reduce the colored noise contribution from ADC when operating with lower bandwidth signals.  Beyond 50 KHz of BW......not much difference exists between the Noise Figure for 16-bit vs 24-bit mode.   Operating with higher VGA settings causes the ADC's colored noise to dominate more.  Refer to figures 11-19 of datasheet.   

    2) Note sure if you mean SSI clock rate vs the IQ rate.   The IQ rate is the ADC clock rate divided by the decimation factor.  Typically one should have the IQ rate be equal or greater than 2x the desired signal bandwidth.   The SSI clock rate can be equal to the ADC clock rate or divided down integer factor of it provided that that the SSI data frame can fit within the time period of the IQ data rate.

Reply
  • Hello,

    Answers to your questions are as follows:

    1)The white noise contribution is from the LNA/VGA/Mixer while the colored noise contribution is from the sigma delta ADC.  Operating with 24-bit  IQ data can reduce the colored noise contribution from ADC when operating with lower bandwidth signals.  Beyond 50 KHz of BW......not much difference exists between the Noise Figure for 16-bit vs 24-bit mode.   Operating with higher VGA settings causes the ADC's colored noise to dominate more.  Refer to figures 11-19 of datasheet.   

    2) Note sure if you mean SSI clock rate vs the IQ rate.   The IQ rate is the ADC clock rate divided by the decimation factor.  Typically one should have the IQ rate be equal or greater than 2x the desired signal bandwidth.   The SSI clock rate can be equal to the ADC clock rate or divided down integer factor of it provided that that the SSI data frame can fit within the time period of the IQ data rate.

Children
  • Hello,

    Thank you for your reply.
    I have an additional question about white noise.
    I would like to know what kind of noise is generated when the PLL is unlocked.
    As an example, when the frequency deviates from a specific frequency with FM radio etc., which frequency component and how many dB does noise occur?
    Best regards,
    Knj

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.