Post Go back to editing

AD9211 output voltage compatibility issue

Am developing a board using AD9211 interfaced with Virtex-5 FPGA. Outputs of the ADC are at LVDS 1.8V and these outputs have to be given to an FPGA bank working at 2.5V. Are these outputs compatible with FPGA 2.5V ?

Parents
  • The output swing of these are compatible, but the common mode voltage voltage may be different.  If the common mode of the receiver lines up with the AD9211, then you can use them directly.  If the common mode of the receiver is higher, you will need to ac couple the outputs to the receiver.  I believe that most receivers will be directly compatible.  

Reply
  • The output swing of these are compatible, but the common mode voltage voltage may be different.  If the common mode of the receiver lines up with the AD9211, then you can use them directly.  If the common mode of the receiver is higher, you will need to ac couple the outputs to the receiver.  I believe that most receivers will be directly compatible.  

Children
No Data