KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
AD1671
Production
The AD1671 is a monolithic 12-bit, 1.25 MSPS analog-to-digital converter with an on-board, high performance sample-and-hold amplifier (SHA) and voltage...
Datasheet
AD1671 on Analog.com
Any ideas on how to reduce the gain error caused by the dc supply voltage. All these add together to make a significant error and I would like to reduce or adjust it out. Can this be helped with the external voltage trim at AIN2 (Pin 22)? Any help is appreciated. Thanks
Hi,
No, I'm not aware of any way to reduce the gain error vs. the supply voltage, that is an internal error that cannot be addressed at the analog inputs. Just need to keep the supplies as accurate and quiet as possible.
Regards,
David
David,
Another question I forgot to ask is how to add these errors. The Vcc and Vlogic are from the same supply so do these errors necessarily add together? Thanks
Hi,
No, the limits on the 5 V supplies can be treated as a single source of error.
Regards,
David