Post Go back to editing

Reset Synchronization of multiple AD12401 (Obsolete) High Speed ADCs

     We have a radar system incorporating five AD12401 400MHz ADCs (now obsolete). We are unable to upgrade to the latest part at this time. There is a well known problem that the reset line does not fully reset all the internal registers for this ADC, so the interleaving of the two flash converters is ambiguous--this leads to synchronization problem, which are especially detrimental in coherent systems.

     We are redoing the FPGA logic utilized in obtaining synchronization, (essentially iterative powering up  the device until the desired state is achieved) but that work was done several years ago and needs updating to a less ad hoc and more reliable process.

Question: Upon application of reset to the AD12401, how can we unambiguously determine the obtained reset state, so we can (externally) swap the output samples to achieve the needed synchronization? A functional discussion or app note dealing with the underlying nature of the reset problem and its detection would be very helpful.

  • When we worked with the original designers of this end application, the quickest solution  available to the customer was to cycle the power until the outputs from each AD12401 came up in the proper order.    Without synchronization you will not know which de-muxed output channel leads or lags on each AD12401 unless you process the output data.   If you know which AD12401 is causing the issue, you can reverse the order for interleaving the output channel data and this should clear up the issue. 

    Another option may be to strobe the DR_EN pin on the AD12401 that is causing the problem.   Strobing the DR_EN pin sets channel A output as the lead channel by restarting the Data Ready outputs with DRA leading DRB.  

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin