Post Go back to editing

"High-Speed" ADC used for single-pulse conversion

Hi guys,

I am looking for a low cost ADC for a single conversion on an external trigger (ECL logic). The trigger comes exactly at the peak amplitude of the pulse (pulse-width < 20ns). I have found the AD9070 which is unfortunately an obsolete product. The digital outputs should be TTL (not ECL) but the conversion-start trigger should be ECL, otherwise (if using an ECL to TTL converter) the maximum amplitude is not hit anymore.

Input voltage range: 0 to 2.5V or 5V

no of bits: 10 or more

the speed of the ADC is not really important as we do not need to detect all pulses (only for monitoring purposes).

any suggestion is welcome!

thx

Parents
  • Hi David,

    thx for the prompt answer!

    the clock cycle latency is not so important as far as I can see, but the timing of the sample&hold circuit, as it has to "freeze"/hold the amplitude value exatcly at the edge of my trigger (which is ECL). If the digital output is delayed this does not matter.

    Actually, due to the high speed S&H circuit, I have posted it in the High-Speed ADC section.

    best regards,

       Hannes

Reply
  • Hi David,

    thx for the prompt answer!

    the clock cycle latency is not so important as far as I can see, but the timing of the sample&hold circuit, as it has to "freeze"/hold the amplitude value exatcly at the edge of my trigger (which is ECL). If the digital output is delayed this does not matter.

    Actually, due to the high speed S&H circuit, I have posted it in the High-Speed ADC section.

    best regards,

       Hannes

Children
No Data