AD9467-FMC-250EBZ clock options

Hi,

I am using AD9467-FMC-250EBZ with ZedBoard. The reference design works with 250 MHz external clock.

  • What are the other options for clocking the AD9467-FMC-250EBZ? Can you explain all options, please?

         

    • How can I use the on board oscillator?
    • How can I use 10 MHz external ref clock to generate 250 MHz clock with AD9517?

Thanks,

Muhammet

Parents
  • Hi,

    Thank you for your reply. As I mentioned before, I want to make minimum modification on PCB. I will use 10MHz reference input from CLK_IN. So, is it possible to use differential reference input to the AD9517 without removing T200 and C204.

    I will just populate C300, C301, C304, C305 and remove C209, C210.

    Thanks in advance,

    Muhammet

Reply
  • Hi,

    Thank you for your reply. As I mentioned before, I want to make minimum modification on PCB. I will use 10MHz reference input from CLK_IN. So, is it possible to use differential reference input to the AD9517 without removing T200 and C204.

    I will just populate C300, C301, C304, C305 and remove C209, C210.

    Thanks in advance,

    Muhammet

Children
No Data