Hello,
In AD9862 data sheet there description that have tree transmit applications section.
Now, i need turn to Two Independent Real Signal DAC Data mode.
What should I do?
AD9862
Obsolete
The AD9860Â / AD9862 are versatile integrated mixed signal front ends that are optimized for broadband wireless applications. The AD9860 / AD9862 are cost...
Datasheet
AD9862 on Analog.com
Hello,
In AD9862 data sheet there description that have tree transmit applications section.
Now, i need turn to Two Independent Real Signal DAC Data mode.
What should I do?
Moving this post to the Data Converter community. Not sure if it should land in High Speed ADCs or High Speed DACs since it is a mixed signal front-end.
Mr Wow,
The Ad9862 is not reccomened for new designs so we can't answer real signal questions. You should consider using the AD9963 which is still reccomended for new designs which has two DACs that can be real.