ADC AD9625 evaluation board Power supply

Hi,

In the ADC AD9625 evaluation board

1) The IO power supply DVDD_IO & SPI_DVDD_IO is 3.3V.

      But recommended voltage is minimum 2.4V to maximum 2.6V.

2) The AVDD1, DRVDD1 & DVDD1 is 1.2V in the schematics

    But the recommended voltage is 1.26V min to 1.32 max.

I planned to use 1.3V & 2.5V for this ADC. what will be the effect ?

Regards

Soumya

Parents
  • 0
    •  Analog Employees 
    on Jul 24, 2014 6:36 PM

    Hi Soumya-

    1) The evaluation board for AD9625 does have support for 3.3V on DVDD_IO & SPI_DVDD_IO.  The datasheet for AD9625 will only specify 2.4 to 2.6V for these domains.  The 3.3V support may be added in the future, but will not be reflected in the released datasheet at this time.

    2) The datasheet will show 1.26Vmin and 1.32V max for AVDD1, DRVDD1 & DVDD1.  This is the final characterized operating range for the release of AD9625.

    Your use of 1.3V and 2.5V respectively will be correct for the operating range of the AD9625.


    Thanks,

    Ian Beavers

Reply
  • 0
    •  Analog Employees 
    on Jul 24, 2014 6:36 PM

    Hi Soumya-

    1) The evaluation board for AD9625 does have support for 3.3V on DVDD_IO & SPI_DVDD_IO.  The datasheet for AD9625 will only specify 2.4 to 2.6V for these domains.  The 3.3V support may be added in the future, but will not be reflected in the released datasheet at this time.

    2) The datasheet will show 1.26Vmin and 1.32V max for AVDD1, DRVDD1 & DVDD1.  This is the final characterized operating range for the release of AD9625.

    Your use of 1.3V and 2.5V respectively will be correct for the operating range of the AD9625.


    Thanks,

    Ian Beavers

Children
No Data