Post Go back to editing

AD9467

Hello

I am having problems with an analyze of the AD9567 NATIVE FMC BOARD.

The AD9467 have 16bit output and can run up to 250MSPs

The output is differential, but i does only have 8 outputs. (8+ and 8 - differential)

so

D1−/D0−   

D1+/D0+    

How do you read the data from D0 and D1 when they share the same differential pins ?

Sorry if it is a stupid question.

Parents
  • Thanks for a great answer,  i think i was confused about the timing diagram on figure 2 on page 7 before, but i makes more sense now.

    One last question.

    The 2 output bits on each differential pair, do i read it right, from the timing diagram, that it is the highest bit that comes first?

    For Example. the differential pair 15 and 14 , it will be bit 15 that comes out first and then bit 14 after ?

    Thanks a lot for the help!

    Max Møller

Reply
  • Thanks for a great answer,  i think i was confused about the timing diagram on figure 2 on page 7 before, but i makes more sense now.

    One last question.

    The 2 output bits on each differential pair, do i read it right, from the timing diagram, that it is the highest bit that comes first?

    For Example. the differential pair 15 and 14 , it will be bit 15 that comes out first and then bit 14 after ?

    Thanks a lot for the help!

    Max Møller

Children
No Data