Hi,
AD9262/AD9267 are not recommended for new designs with no replacements proposal. What would you recommend as CTSD ADC with similar performance?
Regards,
Ivan
AD9262
Not Recommended for New Designs
The AD9262 is a dual, 16-bit analog-to-digital converter (ADC)
based on a continuous time sigma-delta (S-?) architecture that
achieves -87 dB of dynamic...
Datasheet
AD9262 on Analog.com
AD9267
Not Recommended for New Designs
The AD9267 is a dual continuous time (CT) sigma-delta (S-?)
modulator with -88 dBc of dynamic range over 10 MHz real or 20 MHz complex bandwidth. The combination...
Datasheet
AD9267 on Analog.com
Hi,
AD9262/AD9267 are not recommended for new designs with no replacements proposal. What would you recommend as CTSD ADC with similar performance?
Regards,
Ivan
Hello,
The AD9650 would be a suitable replacement since it can achieve low level SNR performance of 83 dBFS @ 100 MSPS (or -160 dBFS/Hz NSD) with spurious below -100 dBFS for baseband signals. If one operates the AD9650 with higher oversampling ratio to reduce anti-aliasing requirements, then decimate in the FPGA is required to reduced data rate to a level that the AD9262 would have provided. Regards.
Hi,
Thank you for the recommendation.
Regards,
Ivan