I am using AD9272-65EBZ with HSC-ADC-EVALCZ.
I would like to increase sampling rate, so I looked over from the website below:
http://www.analog.com/en/products/application-specific/medical/ultrasound.html
I think AD9670 is superior to 9272 in every specs.
I am thinking about buying either of AD9670EBZ or AD9674EBZ.
I compared spec sheet, it seems the only difference between them is demodulator. However, the block diagram is same.
I have 2 questions.
1. what is the other main difference between AD9670ebz and AD9674ebz? I main use is collecting ultrasound signal of 10Mhz or 20Mhz.
2. Are they compatible with HSC-ADC-EVALCZ?
Thanks.