Post Go back to editing

AD9874 LO input impedance

Hello,
We are using AD9874 IF Digitizing chip for down conversion.

We are using discrete VCO for generation of LO of frequency 41.85MHz, to the LO input (LOP) of the AD09874.
When connected the Buffer Amplifier (SGA2463Z) between VCO output and LO input, observed that it is loading the VCO and its frequency is drifting by about 2 MHz.

Please let us know what is the recommended buffer amplifier?
What is the input impedance of LO input for the AD98974?

Parents
  • Hello,

    An equivalent circuit of the AD9874 LO buffer is shown in figure 6 of the datasheet.   The SGA2463Z is an RF 20 dB gain block thus would not represent the best choice for a VCO buffer given its high gain which may result in overdriving the AD9874's LO input and its low input impedance (if directly connected to the VCO tank)..   A simpler approach for 41.85 MHz LO buffer would be to use a simple npn transistor configured as a buffer (i.e. common collector having gain slightly less than 1).  Alternatively, you could use a dedicated IC like the MAX2470/MAX2471 series.

    *Note, most VCO off-the-shelf components include a buffer that isolates the tank from the load thus reducing frequency pulling to load changes.   

Reply
  • Hello,

    An equivalent circuit of the AD9874 LO buffer is shown in figure 6 of the datasheet.   The SGA2463Z is an RF 20 dB gain block thus would not represent the best choice for a VCO buffer given its high gain which may result in overdriving the AD9874's LO input and its low input impedance (if directly connected to the VCO tank)..   A simpler approach for 41.85 MHz LO buffer would be to use a simple npn transistor configured as a buffer (i.e. common collector having gain slightly less than 1).  Alternatively, you could use a dedicated IC like the MAX2470/MAX2471 series.

    *Note, most VCO off-the-shelf components include a buffer that isolates the tank from the load thus reducing frequency pulling to load changes.   

Children
No Data