i have to link the diffierential sinewave output of an ASIC to the analog input of the AD9288.Since it is already a diffierentilal signal,I think maybe i dont need a transformer。So,if i link them with the transmission line by AC coupling,and the differential impedance
of the transmission line is 100 ohm。Should I use an 100 ohm Resistor make the shunt connection between the diffierential analog input of the AD9288 ?