Dear Sir/Madam,
I have an issue about AD10242,.
I wonder whether the encode input could accept ECL signal or LVPECL signal.
what's the input range for the encode of AD10242.
thanks.
BR,
Peng
AD10242
Obsolete
The AD10242 is a complete dual signal chain solution including on-board amplifiers, references, ADCs, and output buffering providing unsurpassed total...
Datasheet
AD10242 on Analog.com
Dear Sir/Madam,
I have an issue about AD10242,.
I wonder whether the encode input could accept ECL signal or LVPECL signal.
what's the input range for the encode of AD10242.
thanks.
BR,
Peng
Hello,
The AD10242 has a logic compatibility for only TTL/CMOS. The Logic Low level must be between 0 - 0.8 Volts and the logic High must be between 2.0 to 5.0 Volts.
John
Hello,
The AD10242 has a logic compatibility for only TTL/CMOS. The Logic Low level must be between 0 - 0.8 Volts and the logic High must be between 2.0 to 5.0 Volts.
John