AD9251 Evaluation: the minimum signal frequency

I bought a HSC-ADC-EVALCZ capture board plus a AD9251 EVL. In my project, the signal frequency which need to be sampled is below 30KHz.

Now, I have a problem. It is found that the signal frequency below 76KHz could not be sampled accurately; I have attaced some results. The signal frequency is 26 KHz, 66KHz and 76KHz. In this case,the sampling rate is set to be 20MHz.

So, I want to know what is the minimum signal frequency that could be sampled accurately by AD9251 EVL. Meanwhile, if AD9251 EVL could not satify me, could you please reconmend another A/D product. 

Thank you so much!

Parents
  • 0
    •  Analog Employees 
    on Aug 16, 2016 10:12 PM

    Hi Yunqi,

    An example of how to modify the board is attached. The original schematic can be found in UG-003 on www.analog.com .

    Here is a very incomplete discussion on the possible effect on performance.

    A portion of noise coupling to a differential signal will affect both components of the signal, which is common mode noise. A large portion of this noise is naturally rejected by the ADC. This modification requires going to a single-ended signal at the ADC inputs. Noise coupled to a single-ended signal will not be rejected in the same way.

    Also, this modification causes what previously were the inverting and non-inverting sides not to match with each other, looking back from the ADC inputs. This could also affect ADC performance.

    The board was originally designed for differential signaling, which is best for AC performance. Changing to single-ended could affect SNR, SINAD, SFDR and linearity, as well as other parameters.

    Thanks,

    Doug

    AD9251_DC_SingleEnded_input_mods.pdf
Reply
  • 0
    •  Analog Employees 
    on Aug 16, 2016 10:12 PM

    Hi Yunqi,

    An example of how to modify the board is attached. The original schematic can be found in UG-003 on www.analog.com .

    Here is a very incomplete discussion on the possible effect on performance.

    A portion of noise coupling to a differential signal will affect both components of the signal, which is common mode noise. A large portion of this noise is naturally rejected by the ADC. This modification requires going to a single-ended signal at the ADC inputs. Noise coupled to a single-ended signal will not be rejected in the same way.

    Also, this modification causes what previously were the inverting and non-inverting sides not to match with each other, looking back from the ADC inputs. This could also affect ADC performance.

    The board was originally designed for differential signaling, which is best for AC performance. Changing to single-ended could affect SNR, SINAD, SFDR and linearity, as well as other parameters.

    Thanks,

    Doug

    AD9251_DC_SingleEnded_input_mods.pdf
Children