Our application is a narrow band I/Q signal at around 2.6MHz, that seems to fall on the input range of the IF2 signal in AD9874.
Can we bypass the LNA and mixer front end of the AD9874 and just use the bandpass sigma delta ADC in AD9874 by directly feeding the signal to the IF2 port?