Input configuration in AD6655 Evaluation Board

Hello everybody,

I want to use AD6655 EVB with a 130 MHz clock signal for sampling a 15MHz bandwidth signal centered around 400MHz. As I have read in the AD6655 datasheet (page nº30) several input configurations are recommended depending on the frequency input range. What input signal configuration is implemented in the evaluation board? Could it be used with the input signal I described above?

Thank you and kind regards