Does AD9234-1000EVM support 1.25GSPS/12.5Gbps lane rates i.e. Max switching characteristics shown in data sheet at Nominal operating conditions ?
I have these ADC cards, Are these cards reliable for 12.5Gbps JESD204B data rates analysis ?
AD9234
Recommended for New Designs
The AD9234 is a dual, 12-bit, 1 GSPS/500 MSPS ADC. The device has an on-chip buffer and sample-and-hold circuit designed for low power, small size, and...
Datasheet
AD9234 on Analog.com
Does AD9234-1000EVM support 1.25GSPS/12.5Gbps lane rates i.e. Max switching characteristics shown in data sheet at Nominal operating conditions ?
I have these ADC cards, Are these cards reliable for 12.5Gbps JESD204B data rates analysis ?
Can anyone from Analog Device comment on this query ? Are AD9234-1000 EBZ cards reliable for 1.25GSPS/12.5Gbps (Max rates) at nominal conditions ??
Hi,
I am not sure what your end goal here is. The AD9234 is rated for a max clock rate of 1GSPS. Please see the AD9234 datasheet for more information. If you want 12.5Gbps line rate, ie, if that is ALL you are looking for, you can clock the AD9234 at 1.25GSPS and get data output at 12.5Gbps. However, dont expect the ADC performance to hold up to datasheet specs.
For 1.25GSPS operation, please use AD9680-1250EBZ. This chip outputs data at 12.5Gbps. The AD9691 is a eight lane version of the same chip. So you have the flexibility to either use eight lanes at 6.25Gbps/lane or four lanes at 12.5Gbps.
The Above Max switching specification of AD9234 mentions about Data rate per channel (NRZ) supports upto @12.5Gbps max.
Since I am still abiding within the ADC datasheet performance ratings mentioned in here would like to know reliability.
Yes,I am clocking the AD9234 upto 1.25GSPS.
The end goal here is to run our Soft JESD204BRX cores interop's on our new upcoming FPGA platform with transceiver's supporting upto 12.7Gbps using AD9234-1000 EBZ cards.
Thanks and Regards,
Shafi
Like i mentioned in my reply above, "If you want 12.5Gbps line rate, ie, if that is ALL you are looking for, you can clock the AD9234 at 1.25GSPS and get data output at 12.5Gbps. However, dont expect the ADC performance to hold up to datasheet specs.
For 1.25GSPS operation, please use AD9680-1250EBZ. This chip outputs data at 12.5Gbps."