AD9265 cmos clock driver

How can i interface AD9265 with CMOS single ended clock driver without using transformer ?

do i need a clock driver ? actually i am driving my clock from FPGA cyclone V.

Do you have any design file which interface this adc to cyclone V ?

What differential amplifier should i use for single ended analog input (AD8375/AD8370/ADA4938) ?

Parents
  • My signal is IF signal at 10.7MHz, which can go -50dBm to 0 dBm.

    I am thinking to use AD9650 instead of AD9265.

    to convert single ended to differential i am planning to use ADA4938.

    I will add 10dB gain by using ADA4938.

    How much max gain ADA4938 can provide ?

    for clock, I am generating clock through CDCM6208 which is having low jitter.

    Now can you suggest me, shall i use balun or transformer after the ADA4938 (before the ADC analog input) ?

    for clock input to adc, shall i use balun too ?

Reply
  • My signal is IF signal at 10.7MHz, which can go -50dBm to 0 dBm.

    I am thinking to use AD9650 instead of AD9265.

    to convert single ended to differential i am planning to use ADA4938.

    I will add 10dB gain by using ADA4938.

    How much max gain ADA4938 can provide ?

    for clock, I am generating clock through CDCM6208 which is having low jitter.

    Now can you suggest me, shall i use balun or transformer after the ADA4938 (before the ADC analog input) ?

    for clock input to adc, shall i use balun too ?

Children
No Data