Hello
How should I provide a 65MHz clock for the AD9248 ADC?
is there any chips or solution boards?
Thanks
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
AD9248
Production
The AD9248 is a dual, 3 V, 14-bit, 20/40/65 MSPS analog to digital converter. It features dual high performance sample-and-hold amplifiers and an integrated...
Datasheet
AD9248 on Analog.com
Hello
How should I provide a 65MHz clock for the AD9248 ADC?
is there any chips or solution boards?
Thanks
Are you using a demo board or did you design your own board? If you have a demo board you can use a single generator to provide the clock, be sure you filter it. If you have a VCXO at 65MHz you can use that. If you use a clock generating device like a AD9510 you can use that as well.