AD9208 Capture Issue @ 2625MHz Clock with ACE and ADS7-V2EBZ

I didn't succeed to capture AD9208 data using the attached test setup and the following test conditions: Fclock = 2625MHz, FPGA global clock = 328.125MHz, Full BW mode, L=8, M=1, F=1, N'=16 (as recommended in the wiki page). The clock signals have generated with an AD9530 PLL evaluation board. I have used this ACE installer version : http://swdownloads.analog.com/ACE/ACEInstall_1.7.2585.1050.exe

ACE Installer Software 1.7.2585.1050 [Sep 15 17]

I have the same issue with an AD6688 eval board. When I click on run once button the SW didn't stop without displaying any error message. Please advice asap as my project is blocked due to this issue ...