Post Go back to editing

How the ADCs like AD9228 or AD9467 start convert?

Hello , I'm meeting a problem. I give a 65MHz diff clock to the clk+ and clk- of a AD9228, However, the Dco ,Fco have no clock output , Dco+  is 1.35V, Dco- is 1V. I don't know how to make Dco and Fco output clock. Is the Dco and Fco output clock automaticly if give the clk pin a input clock?  Please help me!!!

  • Hi

    Are you sure you are providing a clock with enough amplitude at the CLK+/- pins? Do you have an oscilloscope screenshot of the signal measured at the CLK+/- pins? Is the part powered up?

    Thanks

    Umesh

  • Hi UmeshJ,

          Thank u very much for helping me! My oscilloscope screenshot is shown below.The clk+/- pins amplitude are 400mVpp (Blue ones) and 600mVpp (yellow ones)  respectively. The red signal is the result of CH1 sub CH2.

     

  • Hi,

    What is the CM voltage on the CLK+ and CLK- pins? I suppose this is on the AD9228? Is the clock signal AC-coupled? Usually if you clock the chip, the ADC will start converting as long as the power supplies are at the typical level. You can see the DCO clock and the FCO clock.

    Gauging by the screenshot, it seems that the clock differential amplitude is about 1Vpp. is that correct? if so, this amplitude is quite ok for the ADC to start converting. Have you tried to increase the amplitude to see if that might cause the ADC to start converting?

    Thanks

    Umesh

  • Hi UmeshJ,

         Thanks a lot ! Today I replace another chip AD9228,  it's amazing that the Dco+/- can correctly output 390MHz signal(Dco+ as shown Fig1). However , the Fco+/- still have no output, and the data pins output signals (as shown fig2) , the AD9228's input pins are pendent, so is the data pins' signal correct?

         (About CM voltage on the CLK+/- pins)

         I refer to the "Figure 52. Transformer-Coupled Differential Clock" of ad9228's datasheet  for my design,(as shown fig3). I think it is  AC-coupled, However, the datasheet says CLK+/- should have a 1.2V CM voltage(as shown fig4), Why AC- coupled can have CM voltage? My design is wrong ? 

         I think the first problem is make AD9228 output Fco clock , then  i can do next step.

         Please help me!!!

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.