About AD7366 Input Range

Hi,

My customer is trying to use the AD7366.
So I got a question.

#1 As a customer, he seems to want to input 0 to 12 V as an input range.

  In this case, should I set Vdd = + 12 V, Vss = -12 V, reference voltage = 3 V and RANGE 1, 0 both 1?

   

  If I want to select input ranges other than ± 10 V, ± 5 V, 0 V to 10 V, do I select "Do not program" in Table

  8 in the data sheet?
       Is there a proper use of the setting of ± 12 V and 0 V to 12 V?

Best Regards,

Yuya