ACE source code?

Like to see if we can get the source code for ACE. We are working with ADS7-V2 and  AD9208 evaluation board.  Thanks a lot.

Parents
  • Hi Michael,

    Thanks for response.

    Yes, we are looking at possibilities to use Python. Is ACE developed with C or Matlab?

    Also we are looking at adding some new logic to FPGA (on AD9208_ADS7v2) and wondering how an user (via USB port from PC) can control (e.g. via a register write) the logic. From ADS7 schematics, it seems that an user can only communicate with FPGA via Blackfin, right?  I think access to ACE source code may help us to figure it out.    

    Your answer and suggestions are highly appreciated.

    Best,

    Jenny 

Reply
  • Hi Michael,

    Thanks for response.

    Yes, we are looking at possibilities to use Python. Is ACE developed with C or Matlab?

    Also we are looking at adding some new logic to FPGA (on AD9208_ADS7v2) and wondering how an user (via USB port from PC) can control (e.g. via a register write) the logic. From ADS7 schematics, it seems that an user can only communicate with FPGA via Blackfin, right?  I think access to ACE source code may help us to figure it out.    

    Your answer and suggestions are highly appreciated.

    Best,

    Jenny 

Children
No Data