Post Go back to editing

Why AD9864 output is noise when input IF signal is -90dBm

Our product is using AD9864, by out test, when the input IF signal with level of -90dBm directly into AD9864, and the DSP capture AD9864 SSI output IQ data then draw it with Matlab, the data is almost noise, we can't see valid signal. For -70dBm input or -30dBm input, the IQ data looks ok.

So, what's the possible reason for my problem, hardware or AD9864 configuration issue? Could anyone help me? Also I want to know what's the smallest input level that AD9864 can accept.

Here is my AD9864 register setting. And my IF input freq is 73.35MHz, LO freq is 71.1MHz.

Parents
  • Hi PMH,
    I have another question about the AD9864 RSSI. Is there a 24dBm constant gain inside AD9864? For example, I disable VGA and DVAG, also disable the 16dB attenuator, and input a signal with -50dBm. Then I log the SSI IQ data looks like below: (16bit I and 16bit Q, iterative)
    0000 04c6 0000 03ef 0000 040a 0000 04a6 0000 033f 0000 0543 0000 0254 0000 05b0 0000 0162 0000 05fb 0000 0067 0000 0624 0000 ff6b 0000 0624 0000 fe70 0000 05f7
    following the RSSI calculation formula: 10log(I^2+Q^2) = -26dbm. looks like there is a 24dB diff.
    I also tried on other input strength and get the similar result: the calculated RSSI is 24dbm higher than the input signal.
    I am wondering if this is caused by AD9864, but I can't find any description about this in document. Could you help to explain this? Thanks.
Reply
  • Hi PMH,
    I have another question about the AD9864 RSSI. Is there a 24dBm constant gain inside AD9864? For example, I disable VGA and DVAG, also disable the 16dB attenuator, and input a signal with -50dBm. Then I log the SSI IQ data looks like below: (16bit I and 16bit Q, iterative)
    0000 04c6 0000 03ef 0000 040a 0000 04a6 0000 033f 0000 0543 0000 0254 0000 05b0 0000 0162 0000 05fb 0000 0067 0000 0624 0000 ff6b 0000 0624 0000 fe70 0000 05f7
    following the RSSI calculation formula: 10log(I^2+Q^2) = -26dbm. looks like there is a 24dB diff.
    I also tried on other input strength and get the similar result: the calculated RSSI is 24dbm higher than the input signal.
    I am wondering if this is caused by AD9864, but I can't find any description about this in document. Could you help to explain this? Thanks.
Children
No Data