Post Go back to editing

Why AD9864 output is noise when input IF signal is -90dBm

Our product is using AD9864, by out test, when the input IF signal with level of -90dBm directly into AD9864, and the DSP capture AD9864 SSI output IQ data then draw it with Matlab, the data is almost noise, we can't see valid signal. For -70dBm input or -30dBm input, the IQ data looks ok.

So, what's the possible reason for my problem, hardware or AD9864 configuration issue? Could anyone help me? Also I want to know what's the smallest input level that AD9864 can accept.

Here is my AD9864 register setting. And my IF input freq is 73.35MHz, LO freq is 71.1MHz.

Parents
  • FormerMember
    0 FormerMember
on Mar 21, 2018 5:11 PM

Hello,

Thanks for your kind words.  Not sure if any feedback system exists but I am just glad to be helpful.

Regards.

Reply
  • FormerMember
    0 FormerMember
on Mar 21, 2018 5:11 PM

Hello,

Thanks for your kind words.  Not sure if any feedback system exists but I am just glad to be helpful.

Regards.

Children
No Data