AD9864
Production
The AD9864 is a general-purpose IF subsystem that digitizes a
low level, 10 MHz to 300 MHz IF input with a signal bandwidth
ranging from 6.8 kHz to 270...
Datasheet
AD9864 on Analog.com
Our product is using AD9864, by out test, when the input IF signal with level of -90dBm directly into AD9864, and the DSP capture AD9864 SSI output IQ data then draw it with Matlab, the data is almost noise, we can't see valid signal. For -70dBm input or -30dBm input, the IQ data looks ok.
So, what's the possible reason for my problem, hardware or AD9864 configuration issue? Could anyone help me? Also I want to know what's the smallest input level that AD9864 can accept.
Here is my AD9864 register setting. And my IF input freq is 73.35MHz, LO freq is 71.1MHz.
Hello,
1) Updated datasheet is on website................ http://www.analog.com/media/en/technical-documentation/data-sheets/AD6676.pdf.
2) Based on you decimation factor of 900 and SSI frame length of 48...........you should be fine with a clock rate of 1.5 MHz to capture all 48-bits within a frame.
3) The IQ data looks odd for the -30 dBm (and -90 dBm case) since the I and Q waveforms have entirely different envelope characteristics (see plots below). I would advise using simple CW tone that is 1 KHz offset (i.e no modulation) to simply debug. Make sure that the AGC is disabled (0x06=0x0) set CW tone to around -37 dbm level into the AD9864 IF input (i.e. about -8 dBFS for a nominal IF clip point of -31 dBm) such that ADC is several dB below its saturation point. Expectation is that one should see 1 KHz CW tone on both the I and Q output that are 90 degrees out of phase.
Regards.
Hello,
1) Updated datasheet is on website................ http://www.analog.com/media/en/technical-documentation/data-sheets/AD6676.pdf.
2) Based on you decimation factor of 900 and SSI frame length of 48...........you should be fine with a clock rate of 1.5 MHz to capture all 48-bits within a frame.
3) The IQ data looks odd for the -30 dBm (and -90 dBm case) since the I and Q waveforms have entirely different envelope characteristics (see plots below). I would advise using simple CW tone that is 1 KHz offset (i.e no modulation) to simply debug. Make sure that the AGC is disabled (0x06=0x0) set CW tone to around -37 dbm level into the AD9864 IF input (i.e. about -8 dBFS for a nominal IF clip point of -31 dBm) such that ADC is several dB below its saturation point. Expectation is that one should see 1 KHz CW tone on both the I and Q output that are 90 degrees out of phase.
Regards.