Post Go back to editing

Connecting two CS pins. (csa,csb)

Hi. I'm designing my custom board with LTM9010-14.

I will use all 8 channels with same setting.

There are two CS pins , CSA for bank1( ch 1,4,5,8) and CSB for bank2 (ch 2,3,6,7).

Is it okay to tie the two CS (CSA,CSB) pins together?

Does the setting for all channels take place at the same time if two CS pin are tied together?

Or should I set the spi in order for the two banks?

Thanks!