AD7960 analog inputs current

Data sheet, on absolute maximum ratings table, states maximum input current to any pin except supplies is 10mA. However, on page 15 on the section on analog inputs, it says the protection diodes at each input can handle 130mA if the voltage inputs exceed their forward conduction threshold.

So, is it safe to infer the analog inputs can stand a current higher than the 10mA of the aforementioned table?



added question mark
[edited by: EVC at 10:04 PM (GMT 0) on 6 May 2020]
Parents Reply Children