Post Go back to editing

Calculate input power of ADC

According to https://ez.analog.com/b/engineerzone-spotlight/posts/adc-full-scale-input-power I can calculate the input power of a signal sampled with an ADC from the voltage samples with the ADC input impedance. The ADC input impedance is assumed to be 50 Ohm in the linked example.

What is the input impedance I have to use for power conversion of the AD8283 ADC? The data sheet only gives the input impedance for the LNA input (200 Ohm or 2 kOhm), not for the ADC itself. How do I convert the samples to power?

Thanks!

Parents Reply
  • Hi SebMay,

    The input full-scale voltage of the ADC within the AD8283 is 2Vpp_differential, according to the datasheet. This means that a maximum positive output code corresponds to +1V and a minimum negative code corresponds to -1V. If you are capturing the ADC output codes produced by your test signal, this is a way of getting a close representation of the voltage at the ADC inputs.

    Does this help with achieving your goal?

    do you have any other suggestions for SebMay?

    Thank you.

    Doug

Children
  • Hi SebMay, 

    The input seen at the ADC would be an unbuffered switched capacitance input. The impedance would be dependent on the sample rate - so it would change depending on what frequency it is being sampled at or how many channels you are using. 

    I did make a few measurements a while back for 2 and 3 channels, and the differential input impedance varied from 5 to 8 kohms. However, as I mentioned that it is dependent on the sampling frequency, then this will change depending on your configuration.

    I do think that the information at the LNA inputs would be much more predictable. 

    I am not sure whether this gets you closer to what you are trying to calculate. Let me know. 

    Thanks, 

    Kris

  • Hello Dougl, krisf,

    So if I understand that correctly, there is no way how I can deduce the RF input power at the pins of the chip from the voltage samples.

    I would have guessed that there is at least an approximate relationship between the input power and the voltage samples.

    I thought that the voltage samples and the input power were directly proportional to each other.

    Thank you!

  • Hi SebMay,

    It seems to me that what you ask is possible. From the output codes you can get the voltage at the ADC input. If you know the gain of the path from the LNA inputs to the ADC inputs you can derive the approximate voltage at the LNA inputs.

    Do you know the gain settings you are using? Maybe can help with that aspect.

    I know you said that you cannot access the inputs of the AD8283. The AD8283 package is an LFCSP. Aren't the inputs accessible at the package edge? Is the AD8283 beneath some other structures?

    Thank you.

    Doug

  • Hello Dougl,

    the settings I use are:

    16 dB channel gain, 200 Ω input impedance.

    With the devices that I have now available, I do not have acces to the pins. I may be able to get a broken or unused one from a colleague at some point.

    What would I have to do then to calculate the input power?

    Thanks!

  • Hi SebMay,

    Conceptually, if you know the voltage at the ADC input, you can use the gain to calculate what the input is at the IC inputs. Then, if you know the voltage and input resistance at the IC inputs, you can calculate power.

    We'll need to help with understanding the specifics about AD8283 gain and other settings.

    Thanks,

    Doug

  • Hi Sebmay, 

    I agree with what DougL said. If you can deduce the voltage from the output code, you can just divide by the gain you used and calculate using the resistance. That is the probably the best estimate of the power that we can recommend. 

    Thanks, 

    Kris

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.