Post Go back to editing

Calculate input power of ADC

According to https://ez.analog.com/b/engineerzone-spotlight/posts/adc-full-scale-input-power I can calculate the input power of a signal sampled with an ADC from the voltage samples with the ADC input impedance. The ADC input impedance is assumed to be 50 Ohm in the linked example.

What is the input impedance I have to use for power conversion of the AD8283 ADC? The data sheet only gives the input impedance for the LNA input (200 Ohm or 2 kOhm), not for the ADC itself. How do I convert the samples to power?

Thanks!

Parents
  • Hello SebMay, 

    Are you asking for the input so as not to saturate the ADC? You should be fine if you stick to the input voltage on Table 2.

    Please correct me if I am completely misunderstanding the intent of your question! Slight smile

    Thanks, 

    Kris

  • Hello krisf,

    not quite, I am looking for the input impedance of the ADC, because I want to calculate the input power of my signal.

    Here is an example:

    Sinusoidal inuput of 0.25 Vpp, LNA input impedance = 200 Ohm, Vref = 1V

    --> Input power = -14 dBm

    channel gain = 16 dB

    --> Power at the ADC = 2 dBm

    According to your table, this is the maximum input voltage at 16 dB gain, so the ADC would sample a signal with 2 Vpp (1V reference Voltage)

    Then the input impedance of the ADC can be calculated to be ~ 315 Ohm

    Is this correct? Can I use 315 Ohm to convert any sampled signal to power, if I don't know amplitude or power at the input ?

    The input impedance of the ADC changes to 3150 Ohm if I use 2kOhm as input?

    Thank you!

Reply
  • Hello krisf,

    not quite, I am looking for the input impedance of the ADC, because I want to calculate the input power of my signal.

    Here is an example:

    Sinusoidal inuput of 0.25 Vpp, LNA input impedance = 200 Ohm, Vref = 1V

    --> Input power = -14 dBm

    channel gain = 16 dB

    --> Power at the ADC = 2 dBm

    According to your table, this is the maximum input voltage at 16 dB gain, so the ADC would sample a signal with 2 Vpp (1V reference Voltage)

    Then the input impedance of the ADC can be calculated to be ~ 315 Ohm

    Is this correct? Can I use 315 Ohm to convert any sampled signal to power, if I don't know amplitude or power at the input ?

    The input impedance of the ADC changes to 3150 Ohm if I use 2kOhm as input?

    Thank you!

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.