Hi Everybody,
A little bit confuse with the results of the AD7330 in Non Chop Mode at SF=512. As indicate in the papers the Output Rate is equal to ( Mclk/16)*(1/SF), so with SF= 2048 the Output Rate is 150 Hz and SF=512 is 600Hz. That means with lower SF value the lower average of the first filter. How can I convert this Output Rate into Data Output Rate? . I undertand that this is a direct funtion of the resolution for the present analyzed value. For 600 Hz Non Chop Mode the output value will be 15 bits long, that finally wiil give a result of 600/15= 40 values/s . Is is correct?
Thanks and regards from Spain