Hi,
I have 1V input (0.5 offset) connected to AIN pin of the AD9280. The AD9280 is connected as per Figure 18 (Internal Reference - 1 V p-p Input span Top/Bottom mode).
Once I apply the 5V at AVDD and DRVDD, output D7 is stuck at high for about 80 seconds before it starts giving some sensible reading.
different signal on the ADC pin reads as below:
AVDD, DRVDD, MODE - 5V
Clock - works as expected at power up
VREF, REFSENSE, REFTS - 1V
REFTF wrt REFBF -1V.
REFTF wrt 0V = 3V
REFBF wrt 0V = 2V
D7 - 5V
D6 - 0V
D5 - 5V
D4 - 5V
this data line suggests the input is very high which is not. OTR line stays low all the time. TRI and STB lines are always low.
Why I am seeing data out stuck at this level for about sometime before it settles?
Have I got correct mode for the input type?? Please reply as soon as possible. Thanks,,