Low Latency 3.2 G sample/sec (min) ADC for wireless backhaul modem application

Dear Sir,

I need an ADC (dual channel or 2x single channel) with a minimum sampling rate of 3.2 G sample/sec for a very low latency (1GHz bandwidth wireless backhaul modem) to interface with the receive RF side. Please advise best possible candidate ADI high-speed ADC P/N's. Resolution should be >= 8 bits. Most importantly is the latency which should be the lowest possible within ADI portfolio.

For the same project; a DAC (dual channel or 2x single channel) is needed with a minimum sampling rate of 2.4 G sample/sec to interface with the transmit RF side. Please advise best possible candidate ADI high-speed DAC P/N's. Resolution should be >= 10 bits. Most importantly, again, is the latency which should be the lowest possible within ADI portfolio.

Thanks a lot in advance for your support.

KHalid Talaat, Ph.D.

https://www.wasiela.com/

khalid.talaat@wasiela.com