Ad9694 VCM to ADL5205

I would like to use a ADL5205 DC coupled to a AD9694. The default Vocm  of the ADL5205 is Vpos/2 = 1.65 V. The typical VCM for the input of the AD9694 is 1.34 so I intend to use VCM_AB & VCM_CD of the AD9694 to drive the VCM inputs of the ADL5205.

The equivalent circuit of the input to the ADL5205 is approximately a potential divider of two 5 k resistors so to pull this to 1.34 V will require a current of 0.11 mA. We are not told much about the VCM_AB output of the AD9694. 

Can I simply connect the VCM_* outputs of the AD9694 to the VCM inputs of the AD5205? Can it supply this current? Can it drive the recommend 100nF decoupling capacitor at each ADL5205 input?

Thank you,

William

Top Replies