AD9697 and Kintex 7 JESD connection problem

I have AD9697, Kintex 7 and AD9528 for clocking. AD9528 works with SI570 (100 MHz base).
AD9528 gives me 2 clocks 1200 MHz (OUT0 and OUT 13) for ADC and FPGA.

Alsow AD9528 gives m2  2 clocks 120 MHz (OUT2 and OUT 3) for ADC and FPGA for SYS_REF. Additional clk 120 MHz foe FPGA OUT1. This seems well -counters OK.

All screenshots here (AD9528 parameters):

Next stage I setup AD9697:

I want to setup theese parameters JESD:

N'=16, N=14, L=4, M=1, F=1, CS=0, K=32.

What I do:

1) PWDN hard reset  '1' 

2) PWDN hard reset  '0'.

3) Power down  via SPI ( 0002 03) (address and command)

4) Power up  via SPI ( 0002 00) (address and command)

5) Soft reset  0000 81

6) JESD lind down 0571 01

7) NEXT

1228 4F

1228 0F

1222 00

1222 04

1222 00

1262 08

1262 00

8) Setup Link Parameters:

058B 03

058C 00

058D 1F

058E 10

058F 0D

0590 0F

9) JESD lind up 0571 00.

SYNC low((

Top Replies

Parents Reply Children
No Data