Hi,
I am using AD9822 and below is the overall block diagram.
I am using OPAMP circuitry for the front end.

CCD input signal is 2V pkpk (1V to 3V), wherein the reset pulse is 1Vpkpk (2V to 3V) at 1MHz frequency. CDS clocks and ADCCLK are as per the timing diagram.
When the clamp voltage is set to 3V, the output voltage calculated from the output codes has a characteristic as shown below.
The output voltage is around 1.8V and is going to minimum voltage frequently.
Need help in finding what might be the reason for this response.
Also please let me know if CCD works with DC input voltage or not?
Thanks
Pavithra Joshi