Hi,
We brought your AD9278 Evaluation Board and AFE HSC_ADC_EVALC board , and following the "AD9278_79_EVB_User_Guide.pdf" , setting power, setting the SPI control. Then we using an signal synthesizer generate one 1MHz / Vpp=5V sine wave , input to the CH_A, then we run the FFT test on VisualAnalog, but the result show the highest energy signal frequency is around 0.76MHz, at the meantime ,there is no signal around 1MHz.
We also test 5MHz, the final analysis results show the highest energy signal frequency is around 3.8MHz, and the 10MHz input sine signal , final show 7.6MHz signal.
we read the UG sevral times, but still cannot solve this problem , so we need your help.